22.2 Capture Mode
Capture mode uses the 16-bit odd numbered Timer resources (Timer1, Timer3, etc.). When an event occurs on the capture source, the 16-bit CCPRx register captures and stores the 16-bit value of the TMRx register. An event is defined as one of the following and is configured by the MODE bits:
- Every falling edge of CCPx input
 - Every rising edge of CCPx input
 - Every 4th rising edge of CCPx input
 - Every 16th rising edge of CCPx input
 - Every edge of CCPx input (rising or falling)
 
When a capture is made, the Interrupt Request Flag bit CCPxIF of the PIR6 register is set. The interrupt flag must be cleared in software. If another capture occurs before the value in the CCPRx register is read, the old captured value is overwritten by the new captured value.
The following figure shows a simplified diagram of the capture operation.