28.7.2 Endpoint Status - Default Type

This register description is valid for all modes except the Isochronous mode. When the Endpoint Type (TYPE) bit field in the Endpoint Control (EPn.CTRL) register is written to ‘ISO’, see Endpoint Status - Isochronous Type for the correct description.

The Endpoint Status register is modified by the USB hardware. The application modifies this register using the RMW register interface to avoid data hazards. See the “Endpoint Registers – Concurrency and Hazards” section for more details. Flag/status registers in AVR are usually cleared by writing a ‘1’ and can be set only by hardware. These status bits in RAM are an exception where you can write‘0’ to clear them or ‘1’ to set them.

Name: EPn.STATUS
Offset: 0x00 + n*0x08 [n=0..31]
Reset: 0x00

Bit 76543210 
  UNFOVFTRNCOMPLEPSETUPSTALLED BUSNACKTOGGLE 
Access R/WR/WR/WR/WR/WR/W 
Reset xxxxxx 

Bit 6 – UNFOVF Underflow / Overflow Endpoint Flag

The UNF flag is set when an input endpoint is not ready to send data to the host in response to an IN token for input endpoints.

The OVF flag is set when an output endpoint is not ready to accept data from the host following an OUT token for output endpoints.

Bit 5 – TRNCOMPL Transaction Complete Flag

This flag is set when an IN or OUT transaction on the endpoint has successfully completed. When setting this flag, the USB hardware will also set the Transaction Complete (TRNCOMPL) flag in the Interrupt Flags B (INTFLAGSB) register - unless the TRNCOMPL Interrupt Disable (TCDSBL) bit in the Endpoint Control (EPn.CTRL) register is ‘1’.

For multipacket transfers, TRNCOMPL is not set for each transaction but only when a multipacket transfer has been completed.

Bit 4 – EPSETUP Endpoint SETUP Complete Flag

This flag is set when a SETUP transaction has been completed successfully. When this flag is set, all IN and OUT transactions to control endpoints are responded to with a NAK.

This flag must be cleared by the application before decoding the request sent in the setup stage of a control transfer.

Bit 3 – STALLED Endpoint STALL Flag

This flag is set when a STALL handshake has been sent to the host in response to an IN or OUT transaction.

Bit 1 – BUSNACK Data Buffer Not Acknowledge

This flag is set when a packet has been received. When this bit is set the USB peripheral will discard incoming data to the data buffer in an OUT transaction and will not return any data from the data buffer in an IN transaction. For control, bulk and interrupt endpoints a NAK handshake is returned.

After processing the packet, this flag must be cleared by the application. This bit can be written by the application to force returning a NAK to the host, e.g., during initialization. The setting of BUSNACK does not affect the ACKing of SETUP packets.

Bit 0 – TOGGLE Data Toggle

This indicates if a DATA0 or DATA1 PID is expected in the next data packet for an output endpoint, and if a DATA0 or DATA1 PID will be sent in the next transaction for an input endpoint. In most cases, TOGGLE is updated by hardware. The Programming Manual describes the exceptional cases where TOGGLE needs to be updated by the application.

ValueNameDescription
0x0 DATA0 Data packet DATA0
0x1 DATA1 Data packet DATA1