24.3.3.3 32-Bit Input Capture
Two 16-bit Timer/Counter Type B (TCBn) can be combined to work as a true 32-bit input capture.
One TCB is counting the two LSBs. Once this counter reaches MAX, an overflow (OVF) event is generated, and the counter wraps around. The second TCB is configured to count these OVF events and thus provides the two MSBs. The 32-bit counter value is concatenated from the two counter values.
To function as a 32-bit counter, the two TCBs and the system have to be set up as described in the following paragraphs.
System Configuration
- Configure a source (TCA, events, CLK_PER) for the count input for the LSB TCB, according to the application requirements
- Configure the Event System to route the OVF events from the LSB TCB (event generator) to the MSB TCB (event user)
- Configure the Event System to route the same capture event (CAPT) generator to both TCBs
Configuration of the LSB Counter
- Select the configured count input by writing the Clock Select (CLKSEL) bit field in the Control A (CTRLA) register
- Write the Timer Mode (CNTMODE) bit field in the Control B (CTRLB) register to select one of the Input Capture modes
- The Cascade Two Timer/Counters
(CASCADE) bit in CTRLA must be ‘
0’
Configuration of the MSB Counter
- Enable the 32-bit mode by writing the
Cascade Two Timer/Counters (CASCADE) bit in CTRLA to ‘
1’ - Select events as clock input by writing to the Clock Select (CLKSEL) bit field in the Control A (CTRLA) register
- Write the Timer Mode (CNTMODE) bit field in the Control B (CTRLB) register to select the same Input Capture mode as the LSB TCB
Capturing a 32-Bit Counter Value
To acquire a 32-bit counter value, send a CAPT event to both TCBs. Both TCBs are running in the same Capture mode, so each will capture the current counter value (CNT) in the respective Capture/Compare (CCMP) register. The 32-bit capture value is formed by concatenating the two CCMP registers.
Using TCB0 as LSB Counter and TCB1 as MSB Counter
TCB0 is counting the count input, and TCB1 is counting the OVF signals from TCB0. Both TCBs are in Input Capture on Event mode.
A CAPT event is generated and causes both TCB0 and TCB1 to copy their current CNT values to their respective CCMP registers. The two different CASCADE bit values allow a correct timing of the CAPT event.
The captured 32-bit value is concatenated from TCB1.CCMP (MSB) and TCB0.CCMP (LSB).