10.3.2.4 Backup Mode Exit (Wake-up)

The figure below shows the recommended power-up sequence to wake up the SAMA5D2 LPDDR2 SiP from Backup mode. Upon a wake-up event, the Shutdown Controller toggles its SHDN output back to VDDBU to request the power supply to restart. Except for VDDIODDR, DDRM_VDD18 and DDRM_VDD12 which may already be present if the LPDDR2 memory was placed in Self-refresh mode, this power-up sequence is the same one as presented in the figure “Recommended Power-up Sequence”. In particular, the definitions of Group 1 and Group 2 are the same.

Figure 10-4. Recommended Backup Mode Exit (Wake-Up)
Table 10-4. Wake-up Timing Specification
SymbolParameterConditionsMinMaxUnit
t1Group 2 to Group 1 delayDelay from the last Group 2 established(1) supply to the first Group 1 supply turn-on1–ms
t2Group 1 delayDelay from the first Group 1 established supply to the last Group 1 established supply–1
t3DDRM_VDD18 to DDRM_VDD12 delayDelay from the DDRM_VDD18 established to DDRM_VDD12 turn-on0–
t4LPDDR2 power-on delayDelay from DDRM_VDD18 turn-on to DDRM_VDD12 established–20
tRSTPUReset delay at power-upFrom the last established supply to NRST high1–
Note:
  1. An “established” supply refers to a power supply established at 90% of its final value.