5.5.1 Interrupts
5.5.1.1 Introduction
The Interrupt Manager handles and prioritizes the interrupt requests from the different peripheral modules. It also provides APIs for users to control how global, peripheral, and external interrupts will be serviced.
5.5.1.2 Supported Device Families
| PIC12/16F150x | PIC12/16F155x | PIC12/16F157x | PIC12/16F161x |
| PIC12/16F184x | PIC16F145x | PIC16F151x | PIC16F152x |
| PIC16F153xx | PIC16F170x | PIC16F171x | PIC16F176x |
| PIC16F177x | PIC16F178x | PIC16F183xx | PIC16F184xx |
| PIC16F188xx | PIC16F191xx | PIC16F193x | PIC16F194x |
| PIC16LF156x | PIC16LF190x | PIC18F-K40 | PIC18F-Q10 |
5.5.1.3 Required header files
#include "mcc_generated_files/system/interrupt.h"
5.5.1.4 Module Documentation
5.5.1.4.1 INTERRUPT MANAGER
Driver Version
Definitions
-
#define INTERRUPT_GlobalInterruptEnable() (INTCONbits.GIE = 1)
This macro will enable global interrupts.
-
#define INTERRUPT_GlobalInterruptDisable() (INTCONbits.GIE = 0)
This macro will disable global interrupts.
-
#define INTERRUPT_GlobalInterruptStatus() (INTCONbits.GIE)
This macro will return the global interrupt enable bit status.
-
#define INTERRUPT_PeripheralInterruptEnable() (INTCONbits.PEIE = 1)
This macro will enable peripheral interrupts.
-
#define INTERRUPT_PeripheralInterruptDisable() (INTCONbits.PEIE = 0)
This macro will disable peripheral interrupts.
-
#define EXT_INT_InterruptFlagClear() (PIR0bits.INTF = 0)
This routine clears the interrupt flag for the external interrupt, INT.
-
#define EXT_INT_InterruptDisable() (PIE0bits.INTE = 0)
This routine clears the interrupt enable for the external interrupt, INT, and thereafter external interrupts on this pin will not be serviced by the interrupt handler.
-
#define EXT_INT_InterruptEnable() (PIE0bits.INTE = 1)
This routine sets the interrupt enable for the external interrupt, INT, and thereafter external interrupts on this pin will be serviced by the interrupt handler.
-
#define EXT_INT_risingEdgeSet() (INTCONbits.INTEDG = 1)
This routine set the edge detect of the extern interrupt to positive edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a low to high level.
-
#define EXT_INT_fallingEdgeSet() (INTCONbits.INTEDG = 0)
This routine set the edge detect of the extern interrupt to negative edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a high to low level.
Functions
-
void __interrupt ()
This routine services the ISRs of enabled interrupts and is called everytime an interrupt is triggered.
-
void INTERRUPT_Initialize (void)
Initializes Peripheral Interrupt priorities; Enables/disables priority vectors; and, Initializes External Interrupt.
-
void INT_ISR (void)
This ISR will execute whenever the signal on the INT pin will transition to the preconfigured state.
-
void INT_CallBack (void)
Allows for a specific callback function to be called in the INT ISR and allows for a non-specific interrupt handler to be called at runtime.
-
void INT_SetInterruptHandler (void(*InterruptHandler)(void))
Allows selecting an interrupt handler for EXT_INT - INT at application runtime.
-
void INT_DefaultInterruptHandler (void)
This is the default interrupt handler which is called every time the INT ISR is executed and allows any function to be registered at runtime.
Variables
-
void(* INT_InterruptHandler )(void)
This is the dynamic interrupt handler which is called every time the INT ISR is executed and allows any function to be registered at runtime.
Definition Documentation
EXT_INT_fallingEdgeSet
#define EXT_INT_fallingEdgeSet( ) (INTCONbits.INTEDG = 0)
This routine set the edge detect of the extern interrupt to negative edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a high to low level.
|
|
void |
EXT_INT_InterruptDisable
#define EXT_INT_InterruptDisable( ) (PIE0bits.INTE = 0)
This routine clears the interrupt enable for the external interrupt, INT, and thereafter external interrupts on this pin will not be serviced by the interrupt handler.
|
|
void |
EXT_INT_InterruptEnable
#define EXT_INT_InterruptEnable( ) (PIE0bits.INTE = 1)
This routine sets the interrupt enable for the external interrupt, INT, and thereafter external interrupts on this pin will be serviced by the interrupt handler.
|
|
void |
EXT_INT_InterruptFlagClear
#define EXT_INT_InterruptFlagClear( ) (PIR0bits.INTF = 0)
This routine clears the interrupt flag for the external interrupt, INT.
|
|
void |
EXT_INT_risingEdgeSet
#define EXT_INT_risingEdgeSet( ) (INTCONbits.INTEDG = 1)
This routine set the edge detect of the extern interrupt to positive edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a low to high level.
|
|
void |
INTERRUPT_GlobalInterruptDisable
#define INTERRUPT_GlobalInterruptDisable( ) (INTCONbits.GIE = 0)
This macro will disable global interrupts.
|
|
void |
INTERRUPT_GlobalInterruptEnable
#define INTERRUPT_GlobalInterruptEnable( ) (INTCONbits.GIE = 1)
This macro will enable global interrupts.
|
|
void |
INTERRUPT_GlobalInterruptStatus
#define INTERRUPT_GlobalInterruptStatus( ) (INTCONbits.GIE)
This macro will return the global interrupt enable bit status.
|
|
INTERRUPT_PeripheralInterruptDisable
#define INTERRUPT_PeripheralInterruptDisable( ) (INTCONbits.PEIE = 0)
This macro will disable peripheral interrupts.
|
|
void |
INTERRUPT_PeripheralInterruptEnable
#define INTERRUPT_PeripheralInterruptEnable( ) (INTCONbits.PEIE = 1)
This macro will enable peripheral interrupts.
|
|
void |
Function Documentation
__interrupt()
void __interrupt ( )
This routine services the ISRs of enabled interrupts and is called everytime an interrupt is triggered.
|
Interrupt Manager is initialized. |
|
|
void |
INT_CallBack()
void INT_CallBack (void )
Allows for a specific callback function to be called in the INT ISR and allows for a non-specific interrupt handler to be called at runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INT_DefaultInterruptHandler()
void INT_DefaultInterruptHandler (void )
This is the default interrupt handler which is called every time the INT ISR is executed and allows any function to be registered at runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INT_ISR()
void INT_ISR (void )
This ISR will execute whenever the signal on the INT pin will transition to the preconfigured state.
Section: External Interrupt Handlers
|
Interrupt Manager is initialized. |
|
|
void |
INT_SetInterruptHandler()
void INT_SetInterruptHandler (void(*)(void) InterruptHandler)
Allows selecting an interrupt handler for EXT_INT - INT at application runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INTERRUPT_Initialize()
void INTERRUPT_Initialize (void )
Initializes Peripheral Interrupt priorities; Enables/disables priority vectors; and, Initializes External Interrupt.
|
|
void |
Variable Documentation
INT_InterruptHandler
void(* INT_InterruptHandler) (void)
This is the dynamic interrupt handler which is called every time the INT ISR is executed and allows any function to be registered at runtime.
|
Interrupt Manager is initialized. |
|
|
void |
5.5.1.5 File Documentation
5.5.1.5.1 source/interrupt.c File Reference
This file contains the driver code for Interrupt Manager.
#include "../../system/interrupt.h"
#include "../../system/system.h"
Functions
-
void INTERRUPT_Initialize (void)
Initializes Peripheral Interrupt priorities; Enables/disables priority vectors; and, Initializes External Interrupt.
-
void __interrupt ()
This routine services the ISRs of enabled interrupts and is called everytime an interrupt is triggered.
-
void INT_ISR (void)
This ISR will execute whenever the signal on the INT pin will transition to the preconfigured state.
-
void INT_CallBack (void)
Allows for a specific callback function to be called in the INT ISR and allows for a non-specific interrupt handler to be called at runtime.
-
void INT_SetInterruptHandler (void(*InterruptHandler)(void))
Allows selecting an interrupt handler for EXT_INT - INT at application runtime.
-
void INT_DefaultInterruptHandler (void)
This is the default interrupt handler which is called every time the INT ISR is executed and allows any function to be registered at runtime.
Variables
-
void(* INT_InterruptHandler )(void)
This is the dynamic interrupt handler which is called every time the INT ISR is executed and allows any function to be registered at runtime.
Detailed Description
This file contains the driver code for Interrupt Manager.
Interrupt Manager Generated Driver File
5.5.1.5.2 source/interrupt.h File Reference
Functions
-
void INTERRUPT_Initialize (void)
Initializes Peripheral Interrupt priorities; Enables/disables priority vectors; and, Initializes External Interrupt.
-
void INT_ISR (void)
This ISR will execute whenever the signal on the INT pin will transition to the preconfigured state.
-
void INT_CallBack (void)
Allows for a specific callback function to be called in the INT ISR and allows for a non-specific interrupt handler to be called at runtime.
-
void INT_SetInterruptHandler (void(*InterruptHandler)(void))
Allows selecting an interrupt handler for EXT_INT - INT at application runtime.
-
void INT_DefaultInterruptHandler (void)
This is the default interrupt handler which is called every time the INT ISR is executed and allows any function to be registered at runtime.
Macros
-
#define INTERRUPT_GlobalInterruptEnable() (INTCONbits.GIE = 1)
This macro will enable global interrupts.
-
#define INTERRUPT_GlobalInterruptDisable() (INTCONbits.GIE = 0)
This macro will disable global interrupts.
-
#define INTERRUPT_GlobalInterruptStatus() (INTCONbits.GIE)
This macro will return the global interrupt enable bit status.
-
#define INTERRUPT_PeripheralInterruptEnable() (INTCONbits.PEIE = 1)
This macro will enable peripheral interrupts.
-
#define INTERRUPT_PeripheralInterruptDisable() (INTCONbits.PEIE = 0)
This macro will disable peripheral interrupts.
-
#define EXT_INT_InterruptFlagClear() (PIR0bits.INTF = 0)
This routine clears the interrupt flag for the external interrupt, INT.
-
#define EXT_INT_InterruptDisable() (PIE0bits.INTE = 0)
This routine clears the interrupt enable for the external interrupt, INT, and thereafter external interrupts on this pin will not be serviced by the interrupt handler.
-
#define EXT_INT_InterruptEnable() (PIE0bits.INTE = 1)
This routine sets the interrupt enable for the external interrupt, INT, and thereafter external interrupts on this pin will be serviced by the interrupt handler.
-
#define EXT_INT_risingEdgeSet() (INTCONbits.INTEDG = 1)
This routine set the edge detect of the extern interrupt to positive edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a low to high level.
-
#define EXT_INT_fallingEdgeSet() (INTCONbits.INTEDG = 0)
This routine set the edge detect of the extern interrupt to negative edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a high to low level.
Variables
-
void(* INT_InterruptHandler )(void)
This is the dynamic interrupt handler which is called every time the INT ISR is executed and allows any function to be registered at runtime.
Detailed Description
Interrupt Manager Generated Driver API Header File