5.5.3 Interrupts with Vector Table
Interrupt Manager with Interrupt Vector Table (IVT)
5.5.3.1 Introduction
The Interrupt Manager handles and prioritizes the interrupt requests from the different peripheral modules. It also provides APIs for users to control how global, peripheral, and external interrupts will be serviced. This Interrupt Manager module features a Interrupt Vector Table (IVT) which assigns a unique vector address for each interrupt source.
5.5.3.2 Supported Device Families
| PIC18F-Q40 | PIC18F-Q41 | PIC18F-Q43 |
| PIC18F-Q83 | PIC18F-Q84 |
5.5.3.3 Required header files
#include "mcc_generated_files/system/interrupt.h"
5.5.3.4 Module Documentation
5.5.3.4.1 INTERRUPT MANAGER
Driver Version
Definitions
-
#define INTERRUPT_GlobalInterruptHighEnable() (INTCON0bits.GIE = 1)
This macro will enable high priority global interrupts.
-
#define INTERRUPT_GlobalInterruptHighDisable() (INTCON0bits.GIE = 0)
This macro will disable high priority global interrupts.
-
#define INTERRUPT_GlobalInterruptHighStatus() (INTCON0bits.GIE)
This macro will return the global interrupt enable high bit status.
-
#define INTERRUPT_GlobalInterruptLowEnable() (INTCON0bits.GIEL = 1)
This macro will enable low priority global interrupts.
-
#define INTERRUPT_GlobalInterruptLowDisable() (INTCON0bits.GIEL = 0)
This macro will disable low priority global interrupts.
-
#define INTERRUPT_GlobalInterruptLowStatus() (INTCON0bits.GIEL)
This macro will return the global interrupt enable low bit status.
-
#define EXT_INT0_InterruptFlagClear() (PIR1bits.INT0IF = 0)
This routine clears the interrupt flag for the external interrupt, INT0.
-
#define EXT_INT0_InterruptDisable() (PIE1bits.INT0IE = 0)
This routine clears the interrupt enable for the external interrupt, INT0, and thereafter external interrupts on this pin will not be serviced by the interrupt handler.
-
#define EXT_INT0_InterruptEnable() (PIE1bits.INT0IE = 1)
This routine sets the interrupt enable for the external interrupt, INT0, and thereafter external interrupts on this pin will be serviced by the interrupt handler.
-
#define EXT_INT0_risingEdgeSet() (INTCON0bits.INT0EDG = 1)
This routine set the edge detect of the extern interrupt to positive edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a low to high level.
-
#define EXT_INT0_fallingEdgeSet() (INTCON0bits.INT0EDG = 0)
This routine set the edge detect of the extern interrupt to negative edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a high to low level.
-
#define EXT_INT1_InterruptFlagClear() (PIR6bits.INT1IF = 0)
This routine clears the interrupt flag for the external interrupt, INT1.
-
#define EXT_INT1_InterruptDisable() (PIE6bits.INT1IE = 0)
This routine clears the interrupt enable for the external interrupt, INT1, and thereafter external interrupts on this pin will not be serviced by the interrupt handler.
-
#define EXT_INT1_InterruptEnable() (PIE6bits.INT1IE = 1)
This routine sets the interrupt enable for the external interrupt, INT1, and thereafter external interrupts on this pin will be serviced by the interrupt handler.
-
#define EXT_INT1_risingEdgeSet() (INTCON0bits.INT1EDG = 1)
This routine set the edge detect of the extern interrupt to positive edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a low to high level.
-
#define EXT_INT1_fallingEdgeSet() (INTCON0bits.INT1EDG = 0)
This routine set the edge detect of the extern interrupt to negative edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a high to low level.
-
#define EXT_INT2_InterruptFlagClear() (PIR10bits.INT2IF = 0)
This routine clears the interrupt flag for the external interrupt, INT2.
-
#define EXT_INT2_InterruptDisable() (PIE10bits.INT2IE = 0)
This routine clears the interrupt enable for the external interrupt, INT2, and thereafter external interrupts on this pin will not be serviced by the interrupt handler.
-
#define EXT_INT2_InterruptEnable() (PIE10bits.INT2IE = 1)
This routine sets the interrupt enable for the external interrupt, INT2, and thereafter external interrupts on this pin will be serviced by the interrupt handler.
-
#define EXT_INT2_risingEdgeSet() (INTCON0bits.INT2EDG = 1)
This routine set the edge detect of the extern interrupt to positive edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a low to high level.
-
#define EXT_INT2_fallingEdgeSet() (INTCON0bits.INT2EDG = 0)
This routine set the edge detect of the extern interrupt to negative edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a high to low level.
Functions
-
void __interrupt (irq(INT0), base(8))
This ISR will execute whenever the signal on the INT0 pin will transition to the preconfigured state.
-
void __interrupt (irq(INT1), base(8))
This ISR will execute whenever the signal on the INT1 pin will transition to the preconfigured state.
-
void __interrupt (irq(INT2), base(8))
This ISR will execute whenever the signal on the INT2 pin will transition to the preconfigured state.
-
void INTERRUPT_Initialize (void)
Initializes Peripheral Interrupt priorities; Enables/disables priority vectors; and, Initializes External Interrupt.
-
void INT0_CallBack (void)
Allows for a specific callback function to be called in the INT0 ISR and allows for a non-specific interrupt handler to be called at runtime.
-
void INT0_SetInterruptHandler (void(*InterruptHandler)(void))
Allows selecting an interrupt handler for EXT_INT0 - INT0 at application runtime.
-
void INT0_DefaultInterruptHandler (void)
This is the default interrupt handler which is called every time the INT0 ISR is executed and allows any function to be registered at runtime.
-
void INT1_CallBack (void)
Allows for a specific callback function to be called in the INT1 ISR and allows for a non-specific interrupt handler to be called at runtime.
-
void INT1_SetInterruptHandler (void(*InterruptHandler)(void))
Allows selecting an interrupt handler for EXT_INT1 - INT1 at application runtime.
-
void INT1_DefaultInterruptHandler (void)
This is the default interrupt handler which is called every time the INT1 ISR is executed and allows any function to be registered at runtime.
-
void INT2_CallBack (void)
Allows for a specific callback function to be called in the INT2 ISR and allows for a non-specific interrupt handler to be called at runtime.
-
void INT2_SetInterruptHandler (void(*InterruptHandler)(void))
Allows selecting an interrupt handler for EXT_INT2 - INT2 at application runtime.
-
void INT2_DefaultInterruptHandler (void)
This is the default interrupt handler which is called every time the INT2 ISR is executed and allows any function to be registered at runtime.
Variables
-
void(* INT0_InterruptHandler )(void)
This is the dynamic interrupt handler which is called every time the INT0 ISR is executed and allows any function to be registered at runtime.
-
void(* INT1_InterruptHandler )(void)
This is the dynamic interrupt handler which is called every time the INT1 ISR is executed and allows any function to be registered at runtime.
-
void(* INT2_InterruptHandler )(void)
This is the dynamic interrupt handler which is called every time the INT2 ISR is executed and allows any function to be registered at runtime.
Definition Documentation
EXT_INT0_fallingEdgeSet
#define EXT_INT0_fallingEdgeSet( ) (INTCON0bits.INT0EDG = 0)
This routine set the edge detect of the extern interrupt to negative edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a high to low level.
|
|
void |
EXT_INT0_InterruptDisable
#define EXT_INT0_InterruptDisable( ) (PIE1bits.INT0IE = 0)
This routine clears the interrupt enable for the external interrupt, INT0, and thereafter external interrupts on this pin will not be serviced by the interrupt handler.
|
|
void |
EXT_INT0_InterruptEnable
#define EXT_INT0_InterruptEnable( ) (PIE1bits.INT0IE = 1)
This routine sets the interrupt enable for the external interrupt, INT0, and thereafter external interrupts on this pin will be serviced by the interrupt handler.
|
|
void |
EXT_INT0_InterruptFlagClear
#define EXT_INT0_InterruptFlagClear( ) (PIR1bits.INT0IF = 0)
This routine clears the interrupt flag for the external interrupt, INT0.
|
|
void |
EXT_INT0_risingEdgeSet
#define EXT_INT0_risingEdgeSet( ) (INTCON0bits.INT0EDG = 1)
This routine set the edge detect of the extern interrupt to positive edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a low to high level.
|
|
void |
EXT_INT1_fallingEdgeSet
#define EXT_INT1_fallingEdgeSet( ) (INTCON0bits.INT1EDG = 0)
This routine set the edge detect of the extern interrupt to negative edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a high to low level.
|
|
void |
EXT_INT1_InterruptDisable
#define EXT_INT1_InterruptDisable( ) (PIE6bits.INT1IE = 0)
This routine clears the interrupt enable for the external interrupt, INT1, and thereafter external interrupts on this pin will not be serviced by the interrupt handler.
|
|
void |
EXT_INT1_InterruptEnable
#define EXT_INT1_InterruptEnable( ) (PIE6bits.INT1IE = 1)
This routine sets the interrupt enable for the external interrupt, INT1, and thereafter external interrupts on this pin will be serviced by the interrupt handler.
|
|
void |
EXT_INT1_InterruptFlagClear
#define EXT_INT1_InterruptFlagClear( ) (PIR6bits.INT1IF = 0)
This routine clears the interrupt flag for the external interrupt, INT1.
|
|
void |
EXT_INT1_risingEdgeSet
#define EXT_INT1_risingEdgeSet( ) (INTCON0bits.INT1EDG = 1)
This routine set the edge detect of the extern interrupt to positive edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a low to high level.
|
|
void |
EXT_INT2_fallingEdgeSet
#define EXT_INT2_fallingEdgeSet( ) (INTCON0bits.INT2EDG = 0)
This routine set the edge detect of the extern interrupt to negative edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a high to low level.
|
|
void |
EXT_INT2_InterruptDisable
#define EXT_INT2_InterruptDisable( ) (PIE10bits.INT2IE = 0)
This routine clears the interrupt enable for the external interrupt, INT2, and thereafter external interrupts on this pin will not be serviced by the interrupt handler.
|
|
void |
EXT_INT2_InterruptEnable
#define EXT_INT2_InterruptEnable( ) (PIE10bits.INT2IE = 1)
This routine sets the interrupt enable for the external interrupt, INT2, and thereafter external interrupts on this pin will be serviced by the interrupt handler.
|
|
void |
EXT_INT2_InterruptFlagClear
#define EXT_INT2_InterruptFlagClear( ) (PIR10bits.INT2IF = 0)
This routine clears the interrupt flag for the external interrupt, INT2.
|
|
void |
EXT_INT2_risingEdgeSet
#define EXT_INT2_risingEdgeSet( ) (INTCON0bits.INT2EDG = 1)
This routine set the edge detect of the extern interrupt to positive edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a low to high level.
|
|
void |
INTERRUPT_GlobalInterruptHighDisable
#define INTERRUPT_GlobalInterruptHighDisable( ) (INTCON0bits.GIE = 0)
This macro will disable high priority global interrupts.
|
|
void |
INTERRUPT_GlobalInterruptHighEnable
#define INTERRUPT_GlobalInterruptHighEnable( ) (INTCON0bits.GIE = 1)
This macro will enable high priority global interrupts.
|
|
void |
INTERRUPT_GlobalInterruptHighStatus
#define INTERRUPT_GlobalInterruptHighStatus( ) (INTCON0bits.GIE)
This macro will return the global interrupt enable high bit status.
|
|
INTERRUPT_GlobalInterruptLowDisable
#define INTERRUPT_GlobalInterruptLowDisable( ) (INTCON0bits.GIEL = 0)
This macro will disable low priority global interrupts.
|
|
void |
INTERRUPT_GlobalInterruptLowEnable
#define INTERRUPT_GlobalInterruptLowEnable( ) (INTCON0bits.GIEL = 1)
This macro will enable low priority global interrupts.
|
|
void |
INTERRUPT_GlobalInterruptLowStatus
#define INTERRUPT_GlobalInterruptLowStatus( ) (INTCON0bits.GIEL)
This macro will return the global interrupt enable low bit status.
|
|
Function Documentation
__interrupt()[1/3]
void __interrupt (irq(INT0) , base(8) )
This ISR will execute whenever the signal on the INT0 pin will transition to the preconfigured state.
|
Interrupt Manager is initialized. |
|
|
void |
__interrupt()[2/3]
void __interrupt (irq(INT1) , base(8) )
This ISR will execute whenever the signal on the INT1 pin will transition to the preconfigured state.
|
Interrupt Manager is initialized. |
|
|
void |
__interrupt()[3/3]
void __interrupt (irq(INT2) , base(8) )
This ISR will execute whenever the signal on the INT2 pin will transition to the preconfigured state.
|
Interrupt Manager is initialized. |
|
|
void |
INT0_CallBack()
void INT0_CallBack (void )
Allows for a specific callback function to be called in the INT0 ISR and allows for a non-specific interrupt handler to be called at runtime.
Section: External Interrupt Handlers
|
Interrupt Manager is initialized. |
|
|
void |
INT0_DefaultInterruptHandler()
void INT0_DefaultInterruptHandler (void )
This is the default interrupt handler which is called every time the INT0 ISR is executed and allows any function to be registered at runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INT0_SetInterruptHandler()
void INT0_SetInterruptHandler (void(*)(void) InterruptHandler)
Allows selecting an interrupt handler for EXT_INT0 - INT0 at application runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INT1_CallBack()
void INT1_CallBack (void )
Allows for a specific callback function to be called in the INT1 ISR and allows for a non-specific interrupt handler to be called at runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INT1_DefaultInterruptHandler()
void INT1_DefaultInterruptHandler (void )
This is the default interrupt handler which is called every time the INT1 ISR is executed and allows any function to be registered at runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INT1_SetInterruptHandler()
void INT1_SetInterruptHandler (void(*)(void) InterruptHandler)
Allows selecting an interrupt handler for EXT_INT1 - INT1 at application runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INT2_CallBack()
void INT2_CallBack (void )
Allows for a specific callback function to be called in the INT2 ISR and allows for a non-specific interrupt handler to be called at runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INT2_DefaultInterruptHandler()
void INT2_DefaultInterruptHandler (void )
This is the default interrupt handler which is called every time the INT2 ISR is executed and allows any function to be registered at runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INT2_SetInterruptHandler()
void INT2_SetInterruptHandler (void(*)(void) InterruptHandler)
Allows selecting an interrupt handler for EXT_INT2 - INT2 at application runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INTERRUPT_Initialize()
void INTERRUPT_Initialize (void )
Initializes Peripheral Interrupt priorities; Enables/disables priority vectors; and, Initializes External Interrupt.
|
|
void |
Variable Documentation
INT0_InterruptHandler
void(* INT0_InterruptHandler) (void)
This is the dynamic interrupt handler which is called every time the INT0 ISR is executed and allows any function to be registered at runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INT1_InterruptHandler
void(* INT1_InterruptHandler) (void)
This is the dynamic interrupt handler which is called every time the INT1 ISR is executed and allows any function to be registered at runtime.
|
Interrupt Manager is initialized. |
|
|
void |
INT2_InterruptHandler
void(* INT2_InterruptHandler) (void)
This is the dynamic interrupt handler which is called every time the INT2 ISR is executed and allows any function to be registered at runtime.
|
Interrupt Manager is initialized. |
|
|
void |
5.5.3.5 File Documentation
5.5.3.5.1 source/interrupt.c File Reference
This file contains the driver code for Interrupt Manager.
#include "../../system/interrupt.h"
#include "../../system/system.h"
#include <stdbool.h>
Functions
-
void INTERRUPT_Initialize (void)
Initializes Peripheral Interrupt priorities; Enables/disables priority vectors; and, Initializes External Interrupt.
-
void __interrupt (irq(default), base(8))
-
void __interrupt (irq(INT0), base(8))
This ISR will execute whenever the signal on the INT0 pin will transition to the preconfigured state.
-
void INT0_CallBack (void)
Allows for a specific callback function to be called in the INT0 ISR and allows for a non-specific interrupt handler to be called at runtime.
-
void INT0_SetInterruptHandler (void(*InterruptHandler)(void))
Allows selecting an interrupt handler for EXT_INT0 - INT0 at application runtime.
-
void INT0_DefaultInterruptHandler (void)
This is the default interrupt handler which is called every time the INT0 ISR is executed and allows any function to be registered at runtime.
-
void __interrupt (irq(INT1), base(8))
This ISR will execute whenever the signal on the INT1 pin will transition to the preconfigured state.
-
void INT1_CallBack (void)
Allows for a specific callback function to be called in the INT1 ISR and allows for a non-specific interrupt handler to be called at runtime.
-
void INT1_SetInterruptHandler (void(*InterruptHandler)(void))
Allows selecting an interrupt handler for EXT_INT1 - INT1 at application runtime.
-
void INT1_DefaultInterruptHandler (void)
This is the default interrupt handler which is called every time the INT1 ISR is executed and allows any function to be registered at runtime.
-
void __interrupt (irq(INT2), base(8))
This ISR will execute whenever the signal on the INT2 pin will transition to the preconfigured state.
-
void INT2_CallBack (void)
Allows for a specific callback function to be called in the INT2 ISR and allows for a non-specific interrupt handler to be called at runtime.
-
void INT2_SetInterruptHandler (void(*InterruptHandler)(void))
Allows selecting an interrupt handler for EXT_INT2 - INT2 at application runtime.
-
void INT2_DefaultInterruptHandler (void)
This is the default interrupt handler which is called every time the INT2 ISR is executed and allows any function to be registered at runtime.
Variables
-
void(* INT0_InterruptHandler )(void)
This is the dynamic interrupt handler which is called every time the INT0 ISR is executed and allows any function to be registered at runtime.
-
void(* INT1_InterruptHandler )(void)
This is the dynamic interrupt handler which is called every time the INT1 ISR is executed and allows any function to be registered at runtime.
-
void(* INT2_InterruptHandler )(void)
This is the dynamic interrupt handler which is called every time the INT2 ISR is executed and allows any function to be registered at runtime.
Detailed Description
This file contains the driver code for Interrupt Manager.
Interrupt Manager Generated Driver File
5.5.3.5.2 source/interrupt.h File Reference
Functions
-
void INTERRUPT_Initialize (void)
Initializes Peripheral Interrupt priorities; Enables/disables priority vectors; and, Initializes External Interrupt.
-
void INT0_CallBack (void)
Allows for a specific callback function to be called in the INT0 ISR and allows for a non-specific interrupt handler to be called at runtime.
-
void INT0_SetInterruptHandler (void(*InterruptHandler)(void))
Allows selecting an interrupt handler for EXT_INT0 - INT0 at application runtime.
-
void INT0_DefaultInterruptHandler (void)
This is the default interrupt handler which is called every time the INT0 ISR is executed and allows any function to be registered at runtime.
-
void INT1_CallBack (void)
Allows for a specific callback function to be called in the INT1 ISR and allows for a non-specific interrupt handler to be called at runtime.
-
void INT1_SetInterruptHandler (void(*InterruptHandler)(void))
Allows selecting an interrupt handler for EXT_INT1 - INT1 at application runtime.
-
void INT1_DefaultInterruptHandler (void)
This is the default interrupt handler which is called every time the INT1 ISR is executed and allows any function to be registered at runtime.
-
void INT2_CallBack (void)
Allows for a specific callback function to be called in the INT2 ISR and allows for a non-specific interrupt handler to be called at runtime.
-
void INT2_SetInterruptHandler (void(*InterruptHandler)(void))
Allows selecting an interrupt handler for EXT_INT2 - INT2 at application runtime.
-
void INT2_DefaultInterruptHandler (void)
This is the default interrupt handler which is called every time the INT2 ISR is executed and allows any function to be registered at runtime.
Macros
-
#define INTERRUPT_GlobalInterruptHighEnable() (INTCON0bits.GIE = 1)
This macro will enable high priority global interrupts.
-
#define INTERRUPT_GlobalInterruptHighDisable() (INTCON0bits.GIE = 0)
This macro will disable high priority global interrupts.
-
#define INTERRUPT_GlobalInterruptHighStatus() (INTCON0bits.GIE)
This macro will return the global interrupt enable high bit status.
-
#define INTERRUPT_GlobalInterruptLowEnable() (INTCON0bits.GIEL = 1)
This macro will enable low priority global interrupts.
-
#define INTERRUPT_GlobalInterruptLowDisable() (INTCON0bits.GIEL = 0)
This macro will disable low priority global interrupts.
-
#define INTERRUPT_GlobalInterruptLowStatus() (INTCON0bits.GIEL)
This macro will return the global interrupt enable low bit status.
-
#define EXT_INT0_InterruptFlagClear() (PIR1bits.INT0IF = 0)
This routine clears the interrupt flag for the external interrupt, INT0.
-
#define EXT_INT0_InterruptDisable() (PIE1bits.INT0IE = 0)
This routine clears the interrupt enable for the external interrupt, INT0, and thereafter external interrupts on this pin will not be serviced by the interrupt handler.
-
#define EXT_INT0_InterruptEnable() (PIE1bits.INT0IE = 1)
This routine sets the interrupt enable for the external interrupt, INT0, and thereafter external interrupts on this pin will be serviced by the interrupt handler.
-
#define EXT_INT0_risingEdgeSet() (INTCON0bits.INT0EDG = 1)
This routine set the edge detect of the extern interrupt to positive edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a low to high level.
-
#define EXT_INT0_fallingEdgeSet() (INTCON0bits.INT0EDG = 0)
This routine set the edge detect of the extern interrupt to negative edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a high to low level.
-
#define EXT_INT1_InterruptFlagClear() (PIR6bits.INT1IF = 0)
This routine clears the interrupt flag for the external interrupt, INT1.
-
#define EXT_INT1_InterruptDisable() (PIE6bits.INT1IE = 0)
This routine clears the interrupt enable for the external interrupt, INT1, and thereafter external interrupts on this pin will not be serviced by the interrupt handler.
-
#define EXT_INT1_InterruptEnable() (PIE6bits.INT1IE = 1)
This routine sets the interrupt enable for the external interrupt, INT1, and thereafter external interrupts on this pin will be serviced by the interrupt handler.
-
#define EXT_INT1_risingEdgeSet() (INTCON0bits.INT1EDG = 1)
This routine set the edge detect of the extern interrupt to positive edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a low to high level.
-
#define EXT_INT1_fallingEdgeSet() (INTCON0bits.INT1EDG = 0)
This routine set the edge detect of the extern interrupt to negative edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a high to low level.
-
#define EXT_INT2_InterruptFlagClear() (PIR10bits.INT2IF = 0)
This routine clears the interrupt flag for the external interrupt, INT2.
-
#define EXT_INT2_InterruptDisable() (PIE10bits.INT2IE = 0)
This routine clears the interrupt enable for the external interrupt, INT2, and thereafter external interrupts on this pin will not be serviced by the interrupt handler.
-
#define EXT_INT2_InterruptEnable() (PIE10bits.INT2IE = 1)
This routine sets the interrupt enable for the external interrupt, INT2, and thereafter external interrupts on this pin will be serviced by the interrupt handler.
-
#define EXT_INT2_risingEdgeSet() (INTCON0bits.INT2EDG = 1)
This routine set the edge detect of the extern interrupt to positive edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a low to high level.
-
#define EXT_INT2_fallingEdgeSet() (INTCON0bits.INT2EDG = 0)
This routine set the edge detect of the extern interrupt to negative edge, and thereafter interrupt flag will be set when the external interrupt pins level transitions from a high to low level.
Variables
-
void(* INT0_InterruptHandler )(void)
This is the dynamic interrupt handler which is called every time the INT0 ISR is executed and allows any function to be registered at runtime.
-
void(* INT1_InterruptHandler )(void)
This is the dynamic interrupt handler which is called every time the INT1 ISR is executed and allows any function to be registered at runtime.
-
void(* INT2_InterruptHandler )(void)
This is the dynamic interrupt handler which is called every time the INT2 ISR is executed and allows any function to be registered at runtime.
Detailed Description
Interrupt Manager Generated Driver API Header File