5.3.1 6-byte Config Bits Registers
Also includes Fail Safe Clock and Monitoring for Secondary Crystal Oscillator settings
5.3.1.1 Introduction
The MCC Melody Configuration Bits System Driver generates APIs to support device hardware setup on PIC18F-K40 target MCUs.
The Configuration settings allow the user to select the oscillators, reset sources and memory protection from the several options available on the device. They are latched in place at the power-up and also after programming of the device.
5.3.1.2 Supported Device Families
| PIC18F-Q10 | PIC18F-K40 |
5.3.1.3 Required Header Files:
#include "mcc_generated_files/system/config_bits.h"
5.3.1.4 Sample Code
//CONFIG1L
#pragma config FEXTOSC = ECH // External Oscillator Mode Selection->EC (external clock) above 8 MHz; PFM set to high power
#pragma config RSTOSC = EXTOSC // Power-Up Default Value for COSC->EXTOSC operating per FEXTOSC bits (device manufacturing default)
//CONFIG1H
#pragma config CLKOUTEN = OFF // Clock Out Enable->CLKOUT function is disabled
#pragma config FCMEN = ON // Fail-Safe Clock Monitor Enable->Fail-Safe Clock Monitor enabled
#pragma config CSWEN = ON // Clock Switch Enable->Writing to NOSC and NDIV is allowed
//CONFIG2L
#pragma config MCLRE = EXTMCLR // Master Clear (MCLR) Enable->If LVP = 0, MCLR pin is MCLR; If LVP = 1, RG5 pin function is MCLR
#pragma config BOREN = SBORDIS // Brown-Out Reset Enable->Brown-out Reset enabled , SBOREN bit is ignored
#pragma config PWRTE = OFF // Power-Up Timer Enable->Power up timer disabled
#pragma config LPBOREN = OFF // Low-Power BOR Enable->ULPBOR disabled
//CONFIG2H
#pragma config XINST = OFF // Extended Instruction Set Enable->Extended Instruction Set and Indexed Addressing Mode disabled
#pragma config ZCD = OFF // ZCD Disable->ZCD disabled. ZCD can be enabled by setting the ZCDSEN bit of ZCDCON
#pragma config STVREN = ON // Stack Overflow/Underflow Reset Enable->Stack full/underflow will cause Reset
#pragma config BORV = VBOR_2P45 // Brown-out Reset Voltage Selection->Brown-out Reset Voltage (VBOR) set to 2.45V
#pragma config PPS1WAY = ON // PPSLOCKED bit One-Way Set Enable->PPSLOCK bit can be cleared and set only once; PPS registers remain locked after one clear/set cycle
//CONFIG3L
#pragma config WDTCPS = WDTCPS_31 // WDT Period Select->Divider ratio 1:65536; software control of WDTPS
#pragma config WDTE = OFF // WDT Operating Mode->WDT Disabled
//CONFIG3H
#pragma config WDTCWS = WDTCWS_7 // WDT Window Select->window always open (100%); software control; keyed access not required
#pragma config WDTCCS = SC // WDT Input Clock Selector->Software Control
//CONFIG4L
#pragma config WRT1 = OFF // User NVM Self-Write Protection Block 1->Block 1 (004000-007FFFh) not write-protected
#pragma config WRT0 = OFF // User NVM Self-Write Protection Block 0->Block 0 (000800-003FFFh) not write-protected
#pragma config WRT2 = OFF // User NVM Self-Write Protection Block 2->Block 2 (008000-00BFFFh) not write-protected
#pragma config WRT3 = OFF // User NVM Self-Write Protection Block 3->Block 3 (00C000-00FFFFh) not write-protected
#pragma config WRT4 = OFF // User NVM Self-Write Protection Block 4->Block 4 (010000-013FFFh) not write-protected
#pragma config WRT5 = OFF // User NVM Self-Write Protection Block 5->Block 5 (014000-017FFFh) not write-protected
#pragma config WRT6 = OFF // User NVM Self-Write Protection Block 6->Block 6 (018000-01BFFFh) not write-protected
#pragma config WRT7 = OFF // User NVM Self-Write Protection Block 7->Block 7 (01C000-01FFFFh) not write-protected
//CONFIG4H
#pragma config WRTB = OFF // Boot Block Write Protection->Boot Block (000000-0007FFh) not write-protected
#pragma config WRTC = OFF // Configuration Register Write Protection->Configuration registers (300000-30000Bh) not write-protected
#pragma config WRTD = OFF // Data EEPROM Write Protection->Data EEPROM not write-protected
#pragma config LVP = ON // Low Voltage Programming Enable->Low voltage programming enabled. MCLR/VPP pin function is MCLR. MCLRE configuration bit is ignored
#pragma config SCANE = ON // Scanner Enable->Scanner module is available for use, SCANMD bit can control the module
//CONFIG5L
#pragma config CPD = OFF // Data NVM (DFM) Memory Code Protection->DataNVM code protection disabled
#pragma config CP = OFF // User NVM Program Memory Code Protection->UserNVM code protection disabled
//CONFIG6L
#pragma config EBTR1 = OFF // Table Read Protection Block 1->Block 1 (004000-007FFFh) not protected from table reads executed in other blocks
#pragma config EBTR0 = OFF // Table Read Protection Block 0->Block 0 (000800-003FFFh) not protected from table reads executed in other blocks
#pragma config EBTR3 = OFF // Table Read Protection Block 3->Block 3 (00C000-00FFFFh) not protected from table reads executed in other blocks
#pragma config EBTR2 = OFF // Table Read Protection Block 2->Block 2 (008000-00BFFFh) not protected from table reads executed in other blocks
#pragma config EBTR6 = OFF // Table Read Protection Block 6->Block 6 (018000-01BFFFh) not protected from table reads executed in other blocks
#pragma config EBTR5 = OFF // Table Read Protection Block 5->Block 5 (014000-017FFFh) not protected from table reads executed in other blocks
#pragma config EBTR4 = OFF // Table Read Protection Block 4->Block 4 (010000-013FFFh) not protected from table reads executed in other blocks
#pragma config EBTR7 = OFF // Table Read Protection Block 7->Block 7 (01C000-01FFFFh) not protected from table reads executed in other blocks
//CONFIG6H
#pragma config EBTRB = OFF // Boot Block Table Read Protection->Boot Block (000000-0007FFh) not protected from table reads executed in other blocks
5.3.1.5 Module Documentation
5.3.1.5.1 CONFIGBITS Driver
This file contains the API prototype for the Configuration Bits driver.
Module description
This file contains the API prototype for the Configuration Bits driver.
5.3.1.5.2 System Driver
This file contains the API prototype for the System Driver.
Module description
This file contains the API prototype for the System Driver.
Functions
void SYSTEM_Initialize (void)
Initializes the system module. This routine is called only once during system initialization, before calling other APIs.
Function Documentation
SYSTEM_Initialize()
void SYSTEM_Initialize (void )
Initializes the system module. This routine is called only once during system initialization, before calling other APIs.
| None. |
None. |
5.3.1.6 File Documentation
5.3.1.6.1 source/config_bits.c File Reference
This file contains the API Implementation for the Device Configuration Bits driver.
Detailed Description
This file contains the API Implementation for the Device Configuration Bits driver.
Configuration Bits Generated Driver Source File
5.3.1.6.2 source/config_bits.h File Reference
#include "../system/clock.h"
Detailed Description
Configuration Bits Generated Driver Header File
5.3.1.6.3 source/system.c File Reference
This file contains the API implementation for the System driver.
#include "../system.h"
Functions
void SYSTEM_Initialize (void)
Initializes the system module. This routine is called only once during system initialization, before calling other APIs.
Detailed Description
This file contains the API implementation for the System driver.
System Driver Source File
5.3.1.6.4 source/system.h File Reference
#include <xc.h> #include <stdint.h> #include <stdbool.h> #include "config_bits.h" #include "../system/clock.h" #include "../system/pins.h" #include "../system/interrupt.h"
Functions
void SYSTEM_Initialize (void)
Initializes the system module. This routine is called only once during system initialization, before calling other APIs.
Detailed Description
System Driver Header File