9.1.2 HTTP Redirect Feature
The ATWINC15x0 HTTP Provisioning server supports the HTTP redirect feature, which forces all HTTP traffic originating from the associated user device to be redirected to the ATWINC15x0 Provisioning home page.
This simplifies the mechanism of loading the provisioning page instead of typing the exact web address of the HTTP Provisioning server.
To enable this feature, set the redirect flag when calling the API
m2m_wifi_start_provision_mode.
For
further details, refer to the following code example.