14 Reference Documentation
The following table provides the set of collateral documents to ease integration and device ramp.
Title | Content |
---|---|
ATWILC1000/ATWILC3000 Wi-Fi Link Controller Linux® User Guide | This user guide describes how to run Wi-Fi on the ATWILC1000 SD card and how to run Wi-Fi/BLE on the ATWILC3000 Shield board on the SAMA5D4 Xplained Ultra running with the Linux kernel 4.9. |
ATWILC1000B-MU Data sheet | Data sheet for the ATWILC1000 SmartConnect Wi-Fi component. |
ATWILC1000/ATWILC3000 Devices Linux Porting Guide | This user guide describes how to port the ATWILC1000 and ATWILC3000 Linux drivers to another platform and contains all the required modifications for driver porting. |
ATWILC1000/ATWILC3000 Baremetal Wi-Fi/BLE Link Controller Software Design Guide | This design guide helps the user in integrating ATWILC1000/ATWILC3000 in the application using RTOS from Advanced Software Framework (ASF). |
ATWILC1000B/ATWILC1000-MR110xB Errata |
This document provides details on the anomalies identified in the ATWILC1000 family of devices. |
ATWILC1000B – Deriving Application Gain Table Application Note |
This application note describes the Wi-Fi gain table structure and procedure to derive the application gain table. This document provides further details on the steps to update the device with the gain table. |
Note: For a complete listing of development
support tools and documentation, visit http://www.microchip.com/wwwproducts/en/ATWILC1000 or refer to the customer
support section for contacting the nearest Microchip field representative.