1.26.4.21 DBGU_ReadAbort Function

C

/* Non-blocking mode */

bool DBGU_ReadAbort(void)

Summary

Aborts the ongoing read request

Description

This API lets the application abort an ongoing read request. If needed, the application can call the DBGU_ReadCountGet API to know the number of bytes successfully read before issuing the DBGU_ReadAbort API.

Precondition

DBGU_Initialize must have been called for the associated DBGU instance.

Parameters

None

Returns

true - operation is successful

false - error during execution

Example

bool timeout;

if (timeout == true)
{
    // Kill the ongoing read read request
    DBGU_ReadAbort();
}

Remarks

None