1.26.4.20 DBGU_ReadBufferSizeGet Function
C
/* Ring buffer mode */
size_t DBGU_ReadBufferSizeGet(void)
Summary
Returns the size of the receive ring buffer
Description
This function returns the size of the receive ring buffer, which is same as the size of the receive ring buffer configured in MHC.
Precondition
DBGU_Initialize must have been called for the associated DBGU instance.
Parameters
None
Returns
The API returns the size of the receive ring buffer.
Example
size_t rxBufferSize; rxBufferSize = DBGU_ReadBufferSizeGet();
Remarks
None