1.26.4.19 DBGU_ReadByte Function
C
/* Blocking mode */
int DBGU_ReadByte( void )
Summary
Submits request to read a byte of data to the given DBGU peripheral
Description
This function submits request to read a byte of data to the given DBGU peripheral. This Function is available only in blocking mode. Application must call the DBGU_ReceiverIsReady API to check if a byte is available with the receiver before calling this API.
Precondition
-
DBGU_Initialize must have been called for the associated DBGU instance.
-
Receiver readiness must be confirmed using DBGU_ReceiverIsReady.
Parameters
None
Returns
Read byte.
Example
char rxData; if(DBGU1_ReceiverIsReady() == true) { rxData = DBGU1_ReadByte(); }
Remarks
None