1.8.7.73 FLEXCOM_TWI_SLAVE_CALLBACK Typedef
C
/* TWI slave in non-blocking/interrupt mode */ typedef bool (*FLEXCOM_TWI_SLAVE_CALLBACK) ( FLEXCOM_TWI_SLAVE_TRANSFER_EVENT event, uintptr_t contextHandle );
Summary
Defines the data type and function signature for the FLEXCOM TWI Slave callback function.
Description
This data type defines the function signature for the FLEXCOM TWI Slave callback function. The FLEXCOM TWI peripheral will call back the client's function with this signature to report FLEXCOM TWI slave events.
Precondition
FLEXCOMx_TWI_Initialize must have been called for the given FLEXCOM TWI peripheral instance and FLEXCOMx_TWI_CallbackRegister must have been called to set the function to be called. The callback register function should have been called before any transfer is initiated by the I2C master.
Parameters
Param | Description |
---|---|
event | Indicates the data transfer event for which the callback function has been called. |
contextHandle | Allows the caller to provide a context value (usually a pointerto the callers context for multi-instance clients). |
Returns
bool - The return value is ignored by the TWI slave PLIB
Example
void APP_FLEXCOM_TWI_Callback ( FLEXCOM_TWI_SLAVE_TRANSFER_EVENT event, uintptr_t contextHandle ) { switch(event) { case FLEXCOM_TWI_SLAVE_TRANSFER_EVENT_ADDR_MATCH: // Handle address match event break; case FLEXCOM_TWI_SLAVE_TRANSFER_EVENT_RX_READY: // Read the received data byte rxData = FLEXCOM1_TWI_ReadByte(); break; case FLEXCOM_TWI_SLAVE_TRANSFER_EVENT_TX_READY: // Provide data to TWI master FLEXCOM1_TWI_WriteByte(txData); break; case FLEXCOM_TWI_SLAVE_TRANSFER_EVENT_TRANSMISSION_COMPLETE: // Handle stop bit received event break; } } // Register Callback function which is defined above FLEXCOM1_TWI_CallbackRegister(APP_FLEXCOM_TWI_Callback, 0);
Remarks
None