1.8.2.4 ADC_ChannelsInterruptEnable Function
C
void ADC_ChannelsInterruptEnable(ADC_INTERRUPT_MASK channelsInterruptMask) void ADC_ChannelsInterruptEnable(ADC_INTERRUPT_EOC_MASK channelsInterruptMask)
Summary
Enables the ADC interrupt sources
Description
This function enables interrupt sources specified in channelsInterruptMask.
Precondition
ADC_Initialize() must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
channelsInterruptMask | interrupt sources |
Returns
None.
Example
ADC_Initialize();
ADC_ChannelsInterruptEnable(ADC_INTERRUPT_EOC_0_MASK);
Remarks
This function does not disable interrupts which are not included in the mask.