1.26.17.2 SDMMCx_ResponseRead Function
C
/* x = SDMMC instance number */ void SDMMCx_ResponseRead ( SDMMC_READ_RESPONSE_REG respReg, uint32_t* response )
Summary
Reads the response to a given command.
Description
If the command requires a response, it can be read using this API.
Precondition
A command having a response must have been submitted using the SDMMCx_CommandSend() function.
Parameters
Param | Description |
---|---|
respReg | Enumeration of SDMMC_READ_RESPONSE_REG type describing the resonse register to read |
response | Pointer to the buffer to read the response into |
Returns
None.
Example
uint32_t cmd_response;
SDMMC1_ResponseRead(SDMMC_READ_RESP_REG_0, &cmd_response);
Remarks
None.