2.72.5 NVM_SingleDoubleWordWrite Function
C
bool NVM_SingleDoubleWordWrite( uint32_t *data, uint32_t address );
Summary
Writes Two Words into the Flash.
Description
Writes Two Words (8 bytes) at the given address.
Precondition
None
Parameters
Param | Description |
---|---|
data | Pointer to the buffer which holds data to be written. |
address | Address at which the data will be written. |
Returns
Always return true.
Example
uint32_t data[2]; data[0] = 0x12345678; data[1] = 0x87654321; NVM_SingleDoubleWordWrite((uint32_t *)data, 0x9D100000);
Remarks
This Feature may not be available on all devices. Refer to device Datasheet for more information.