2.72.4 NVM_WordWrite Function

C

bool NVM_WordWrite( uint32_t data, const uint32_t address );

Summary

Writes One word into the Flash.

Description

Writes one word (4 bytes) at the given address.

Precondition

None

Parameters

ParamDescription
dataData to be written.
addressAddress at which the data will be written.

Returns

Always return true.

Example

NVM_WordWrite(data_to_fill, 0x9D100000);