2.22.1 CRCCUx_Initialize Function
C
void CRCCUx_Initialize( void ); // x - Instance of the CRCCU peripheral
Summary
Initializes given instance of CRCCU peripheral.
Description
This function initializes given instance of CRCCU peripheral of the device with the values configured in MCC GUI. Once the peripheral is initialized, peripheral can be used for CRC Calculation.
Precondition
MCC GUI should be configured with the right values.
Parameters
None.
Returns
None.
Example
CRCCU_Initialize();
Remarks
This function must be called before any other CRCCU function is called. This function should only be called once during system initialization.