3.2.22 Timer(TMR)
The Timer1 module found in particular family devices shares many features with a classic Type A timer. There is typically a single Timer1 module implemented for each CPU core present in a device. Timers are useful for generating accurate time-based periodic interrupt events for software applications or real-time operating systems. Other uses include counting external pulses or accurate timing measurement of external events by using the timer’s gate feature. The timers found in some particular family devices include the following features:
• Asynchronous and Synchronous Operation
• Software-Selectable Internal or External Clock Sources
• Programmable Interrupt Generation and Priority
• Gated External Pulse Counter
• Software Prescalers: 1:1, 1:8, 1:64 and 1:256
Using The Library
Timer mode is used for periodic interrupt generation. When the timer is enabled, it increments by one on every rising edge of the input clock, and generates an interrupt on a period match and the registered callback function will be called.
Callback method This example demonstrates how to use the timer to generate periodic callback.
/* This function is called after period expires */ void TIMER1_EventHandler(uint32_t status, uintptr_t context) { /* Toggle LED */ LED_Toggle(); } int main(void) { /* Register callback function Timer interrupt */ TMR1_CallbackRegister(TIMER1_EventHandler,(uintptr_t)NULL); /* Start the timer channel 0*/ TMR1_Start(); }
Library Interface
Peripheral library provides the following interfaces:
Functions
| Name | Description |
|---|---|
| TMRx_Initialize | Initializes given instance of TMR |
| TMRx_Deinitialize | De-initializes given instance of TMR |
| TMRx_Start | Starts the given Timer |
| TMRx_Stop | Stops the given Timer counter |
| TMRx_PeriodSet | Sets the period value of a given timer |
| TMRx_PeriodGet | Reads the period value of given timer |
| TMRx_CounterGet | Reads the timer counter value |
| TMRx_FrequencyGet | Provides the given timer's counter-increment frequency |
| TMRx_InterruptEnable | Enable TMR overflow interrupt |
| TMRx_InterruptDisable | Disable TMR overflow interrupt |
| TMRx_CallbackRegister | Sets the callback_fn function for an match |
| TMRx_PeriodHasExpired | Checks period expiration |
| TMRx_StartTimeOut | Stores current tick count and delay value in the timeout |
| TMRx_ResetTimeOut | Resets current tick count in the timeout |
| TMRx_IsTimeoutReached | Checks for timeout |
| TMRx_GetTickCounter | Returns current tick count |
Data types and constants
| Name | Type | Description |
|---|---|---|
| TMR_CALLBACK | Typedef | Defines the function pointer data type and function signature for the TMRx callback function |
| TMR_TIMEOUT | Struct | Defines the following parameters for a timeout period. |