23.3.4 Input/Output Section Map
The last section in the default linker script is the input/output section
map. The section map is the heart of the linker script. It defines how input sections
are mapped to output sections. Note that input sections are portions of an application
that are defined in source code, while output sections are created by the linker.
Generally, several input sections may be combined into a single output section. All
output sections are specified within a SECTIONS command in the linker
script.