23.3.4.2 .Reset Section
This section contains the code that is executed when the processor performs a Reset. This
section is located at the Reset address (_RESET_ADDR), as specified in
the processor definitions linker script and is assigned to the boot memory region
(kseg1_boot_mem). The .reset output section also
contains the C start-up code from the .reset.startup input section.
.reset _RESET_ADDR :
{
KEEP(*(.reset))
KEEP(*(.reset.startup))
} > kseg1_boot_mem