23.3.4.19 .lit4 Section
This section collects the 4-byte constants (usually floating-point) which the
assembler decides to store in memory rather than in the instruction stream from all of
the application’s input files. This section is assigned to the data memory region
(kseg1_data_mem) with a load address located in the program memory
region (kseg0_program_mem). A symbol is defined to represent the
virtual end address of the initialized data (_data_end).
.lit4 :
{
*(.lit4)
} > kseg1_data_mem AT> kseg0_program_mem
_data_end = . ;