23.3.4.4 .dbg_excpt Section
This section reserves space for the debug exception vector. This section is only
allocated if the symbol _DEBUGGER has been defined. (This symbol is
defined if the -mde-bugger command line option is specified to the
shell.) This section is located at the debug exception address
(_DBG_EXCPT_ADDR) as specified in the processor definitions linker
script and is assigned to the boot memory region (kseg1_boot_mem). The
section is marked as NOLOAD as it is only intended to ensure that
application code cannot be placed at locations reserved for the debug executive.
.dbg_excpt _DBG_EXCPT_ADDR (NOLOAD) :
{
. += (DEFINED (_DEBUGGER) ? 0x8 : 0x0);
} > kseg1_boot_mem