3.7.2 Steps to Configure Low-Power
-
Configure the Button n as a Low-Power button by writing
1to the Low-Power Sensor (LP) bit in the Sensor Control (SENCTRL) register.Note: If one or more of the buttons are not set to be low-power buttons, the device will not go into Low-Power mode. - Enable Low-Power mode by writing
1to the Low-Power (LP) bit in the Device Control (DEVCTRL) register.Note: Calibration and Suspension of Button n should not be enabled (Refer to the Sensor Control (SENCTRL) register).
Refer to the Configuration Summary for more details.