36.10.3.2 NCS Waveforms

The NCS signal waveforms in write operations are not the same as those applied in read operations, but are defined separately:

  • NCS_WR_SETUP: the NCS setup time is defined as the setup time of the address before the NCS falling edge.
  • NCS_WR_PULSE: the NCS pulse length is the time between the NCS falling edge and the NCS rising edge.
  • NCS_WR_HOLD: the NCS hold time is defined as the hold time of the address after the NCS rising edge.
Figure 36-10. Write Cycle