37.2.13.1 Error Type TE0
Error Type TE0 occurs when the Target receives an invalid Broadcast Address
7’h7E/W or Dynamic Address/R/W from the
Controller after being assigned a Dynamic Address. When this happens, the Target is
unable to distinguish whether the transfer is a CCC transfer or a Private
R/W transfer. Since it cannot distinguish the CCC transfer,
the Target would be unaware if the Controller enters HDR mode and might attempt to
interpret HDR transfer as though the bus were still in SDR mode, which could become
potentially fatal when not handled properly.
7’h3E / W, 7’h5E
/ W, 7’h6E / W, 7’h76 / W, 7’h7A / W,
7’h7C / W, 7’h7F / W, or 7’h7E /
R. The Target can also detect this error when its own Dynamic Address is invalid on the
bus, however the probability of such a detection is extremely low. The TE0ERR bit and the BUSEIF Bus Error Interrupt Flag are set upon successful detection of TE0
type error. Once set, the TE0ERR and BUSEIF bits will not self-clear. The user must
clear them in software to re-arm the functionality of each bit individually.The Target recovers from this Error condition by enabling the HDR Exit Detector and ignoring the rest of the patterns on the bus. The Target can also auto-recover by forcing the module out of HDR mode. Refer to the Software Force HDR Exit section for more information.