3.3 Importing the Firmware Drivers
(Ask a Question)After the driver files are downloaded, they must be imported into the empty project.
To import the drivers, perform the following steps:
- In SoftConsole, right-click the
MiV_uart_blinky project, and select
Import, as shown in the following figure.
Figure 3-7. Import Option
- In the Import
dialog box, expand the General folder, and double-click
File System, as shown in the following figure.
Figure 3-8. Import Dialog Box
- On the next page of the
Import dialog box, do the following:
- Click Browse, and locate the folder where you downloaded the drivers.
- From the folder, select the drivers, filelist, hal, and miv_rv32_hal folders.
- Click Finish.
Figure 3-9. Import Dialog Box - Page 2
The miv_rv32_hal, hal, and driver files are imported into the MiV_uart_blinky project.