3.3.5.2 DMAC_ChannelIsBusy
Reads the busy status of a channel.
The function returns true if the specified channel is busy with a transfer. This function can be used to poll for the completion of transfer that was started by calling the DMAC_ChannelTransfer() function. This function can be used as a polling alternative to the setting a callback function and receiving an asynchronous notification for transfer notification.
bool
DMAC_ChannelBusy
(
DMAC_CHANNEL channel
);
Precondition
- DMAC should have been initialized by calling the DMAC_Initialize.
Parameters
- channel - the particular channel to be interrogated
Returns
- returns true if the channel is busy with an on-going transfer, otherwise, false if not busy and is available for a transfer.