4.1.4 JTAG Programming Using External Microprocessor
(Ask a Question)An external microprocessor can be used to program the device through the dedicated JTAG interface. This type of programming requires that the external microprocessor run DirectC, a Microchip programming solution for FPGAs, and the microprocessor’s GPIO ports drive the JTAG interface.
Security only bitstream must be programmed only on erased or blank devices. If the security bitstream is used to program a previously programmed FPGA, it disables the FPGA Array. The fabric must be re-programmed to enable it.
The following figure shows a sample implementation of device programming using an external microprocessor running DirectC.