4.1.3 JTAG Programming Using FlashPro Programmer

Microchip FlashPro programmer v5 or later can be used to program RT PolarFire FPGA through the dedicated JTAG interface. This can be done either using the Libero SoC or a standalone FlashPro Express.

The FlashPro programmer connects to the device via a 10-pin programming header using a FlashPro cable (10-pin ribbon), as shown in the following figure.

Figure 4-2. JTAG Programming Using External Programmer

The following table lists the FlashPro header signals.

Table 4-2. FlashPro Header Signals
Pin NumberSignalDirection to FlashPro ProgrammerDescription
1TCK/SCKOutputJTAG/SPI clock.
2GND

Signal reference. GND pins must be connected.
3TDO/MISOInputJTAG/SPI data output from programming device.
4PROG_MODENot connectedUnused
5TMS/SSOutputJTAG test-mode select/SPI slave select.
6VJTAG/VSPI

Target interface voltage input.
7VPUMPNot connectedUnused
8TRSTBOutputJTAG test reset.
9TDI/MOSIOutputJTAG/SPI data input to programming device.
10GND

GND

A single FlashPro programmer can program multiple Microchip FPGAs from the same family or from different families in a single JTAG chain. The TDO pin of the JTAG header represents the beginning of the chain. The TDI pin of the last device connects back to the JTAG header, thus completing the JTAG chain. The following types of FPGAs can be added to a JTAG chain:

  • Microchip devices targeted for programming
  • Microchip bypass devices not targeted for programming
  • Non-Microchip bypass devices

When a device is in Bypass mode, the device’s data register length is automatically set to 1 and the device stops responding to any programming instructions. To place a device in bypass mode, the instruction register (IR) length must be known. For Microchip FPGAs, the IR length is obtained automatically by the FlashPro Express. For non-Microchip FPGAs, the boundary scan description language (BSDL) file, which contains a sequence of boundary scan commands and data, must be loaded, or the IR length must be manually entered in the FlashPro Express. For more information about JTAG chain programming, see FlashPro User’s Guide.

Figure 4-3. Device Programming in JTAG Chain

For information about power supply requirement and filtering capacitors, see UG0726: PolarFire FPGA Board Design User Guide.

The following figure shows the connections between the programming header and the device.

Figure 4-4. Connecting FlashPro Programmer to a Device