2.5.2.3 Hitless Clock Switching: Disable SyncE
(Ask a Question)The following figure shows the Hitless clock switching for disable SyncE.
Whenever the ESMC receiver subsystem receives a new QL-value, the selection algorithm compares the incoming QL-value with the already existing local QL-value and makes the appropriate decision.
If the incoming QL-value has a lower priority than the existing local QL-value, then the selection algorithm notifies the JAPLL Controller to take necessary action such that the JAPLL locks to the better-quality local auxiliary clock and disable the SyncE.
The JAPLL Controller performs the following sequence of steps to disable the SyncE:
- ENTER_HOLDOVER:
- Enable JAPLL hold by setting JA_HOLD to "1" and PRESET_EN to "1" to use the Averaged INT and FRAC preset values.
- WAIT_FOR_VALID_LINK:
- Wait for 200 µs to make sure the JAPLL enters holdover.
- EN_DIS_SYNCE:
- Switch the FIN of JAPLL to the local auxiliary clock.
- Now JAPLL starts locking to the local auxiliary clock.
- EXIT_HOLDOVER:
- Set JA_HOLD to "0" and PRESET_EN to "0" to disable JAPLL hold.
- Stop the averaging algorithm. For more information, see Averaging Algorithm Implementation.