1.5 CCP Timer Mode
This example demonstrates how to use the CCP module in timer mode to generate periodic interrupt.
Description
The CCP module in timer mode generates periodic interrupt on 1 second period match. The LED is toggled in the interrupt handler to indicate periodic callback.
Downloading and building the application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.
Path of the application within the repository is apps/ccp/ccp_timer_mode.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| pic32ak_gc_curiosity.X | MPLABX project for Curiosity Platform Development Board and PIC32AK1216GC41064 General Purpose Dual In-Line Module (DIM) | 
Setting up the hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| pic32ak_gc_curiosity.X | Curiosity Platform Development Board and PIC32AK1216GC41064 General Purpose Dual In-Line Module (DIM) | 
Setting up Curiosity Development Board
- Insert the GP DIM on to DIM slot of Curiosity Board
 - Connect the PKoB (J24) on the board to the computer using a USB type-C cable
 - Connect the logic analyzer to pin 3 (RB3) of XPRO1 Header
 
Running the Application
- Build and program the application project using its IDE
 - On successful execution, LED starts blinking
 - Observe the output on logic analyzer, GPIO pin toggles at 1 HZ frequency
 
| Board | LED Name | GPIO PIN | 
|---|---|---|
| Curiosity Platform Development Board and PIC32AK1216GC41064 General Purpose Dual In-Line Module (DIM) | LED0 | pin 3 (RB3) of XPRO1 Header |