1.14 SENT Receiver
This example demonstrates how to use the SENT module in receiver mode to receive transmitted data.
Description
The SENT module is used as a receiver to receive transmitted data. The LED is set once the reception has succesfully completed. The data to be transmitted is stored in a structure called sentDataTransmit. The data received is stored in a structure called sentDataReceive. It has two data nibbles and one status nibble.
Downloading and building the application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/sent/receiver.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| pic32ak_gc_curiosity.X | MPLABX project for Curiosity Platform Development Board and PIC32AK1216GC41064 General Purpose Dual In-Line | 
Setting up the hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| pic32ak_gc_curiosity.X | Curiosity Platform Development Board and PIC32AK1216GC41064 General Purpose Dual In-Line | 
Setting up Curiosity Platform Development Board
- Insert the GP DIM on to DIM slot of Curiosity Board
 - Connect the PKoB (J21) on the board to the computer using a USB type-C cable
 
Running the application
- Build and program the application project using its IDE
 - On successful execution,
                        intended LED sets.
Board LED Curiosity Development Board LED4, LED3