1.9 DMA Memory Transfer
This example application demonstrates how to use the DMA peripheral to do a memory to memory transfer.
Description
The application uses a software trigger to initiate a memory-memory transfer from the source buffer to the destination buffer with one byte data size. Transfer status is reported on console.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/dma/dma_memory_transfer.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32ak_gc_curiosity.X | MPLABX project forCuriosity Platform Development Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32ak_gc_curiosity.X | Curiosity Platform Development Board |
Setting Up Curiosity Platform Development Board
- Connect a PIC32AK1216GC41064 General Purpose Dual In-Line Module (DIM) to the J1 header
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Open the Terminal application (Ex.: Tera term) on the computer
- Connect to the “USB to UART” COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Build and Program the application project using its IDE
- Following message is output on
console:

- The LED indicates the success or failure:
- The LED is turned ON when
the DMA memory transfer is successfulFollowing table provides LED names:
Board LED Name Curiosity Platform Development Board LED1
- The LED is turned ON when
the DMA memory transfer is successful