1 MPLAB® Harmony 3 Peripheral Library Application Examples for PIC32AK-GC family
The following applications are provided to demonstrate the typical or interesting usage models of one or more peripheral libraries.
| Name | Description | 
|---|---|
| ADC Interrupt | 
                             This example application shows how to sample an analog input using the ADC peripheral and displays the converted samples on a serial terminal in interrupt mode  | 
| ADC Polling | 
                             This example application shows how to sample an analog input using the ADC peripheral and displays the converted samples on a serial terminal in polled mode  | 
| CCP Capture Mode | This example shows how to use the CCP module in capture mode to measure pulse width of an input signal. | 
| CCP Compare Mode | This example shows how to use the CCP module in compare mode to generate an dual edge, active high, and toggle output on compare match. | 
| CCP Timer Mode | This example demonstrates how to use the CCP module in timer mode to generate periodic interrupt. | 
| CLC Manchester Encoder | This example application shows how to use the CLC peripheral library and generate a Manchester-encoded output. | 
| CMP DAC Sine Wave | 
                             This code example demonstrates how to generate a 100 Hz sine wave without CPU intervention using the DMA, DAC and TMR peripherals  | 
| CRC-32 Generation | This example application demonstrates how to use the CRC peripheral to compute 32-bit Cyclic Redundancy Checksum (CRC). | 
| DMA Memory Transfer | This example application demonstrates how to use the DMA peripheral to do a memory to memory transfer | 
| I2C EEPROM Emulation (I2C Client) | 
                             This example application demonstrates how to use the I2C peripheral in client mode.  | 
| I2C EEPROM Read Write | 
                             This example application demonstrates how to use the I2C peripheral to write and read from the I2C serial EEPROM memory  | 
| PTG Interrupt | This example demonstrates how to use PTG to execute different step commands | 
| PWM Generators Synchronous Output | This example application demonstrates how to Synchronize multiple PWM Generators buffer update to get synchronous output | 
| SENT Receiver | This example demonstrates how to use SENT peripheral as a Receiver | 
| SENT Transmitter | This example demonstrates how to use SENT peripheral as a Transmitter | 
| SPI EEPROM Read Write | This example application demonstrates how to use the SPI peripheral to write and read from the SPI serial EEPROM memory | 
| SPI Flash Write Read | This example shows how to use the SPI Peripheral library to perform erase, write and read operation with the SPI Serial Flash memory. | 
| SPI Host Read Write Test Application | This is a SPI Host test application which is provided to demonstrate communication between SPI host and the corresponding SPI client application available under - apps/spi/client/spi_write_read | 
| SPI Client Read Write | This example application demonstrates how to use the SPI peripheral in client mode | 
| Timer Interrupt | This example application demonstrates how to use timer peripheral in interrupt mode to generate periodic interrupts | 
| UART Echo Blocking | This example application demonstrates how to use the UART peripheral to transfer a block of data in a blocking manner | 
| UART Echo Interrupt | 
                             This example application demonstrates how to use the UART peripheral to transfer a block of data in a non-blocking manner  | 
| UART Ring Buffer | 
                             This example application demonstrates how to use the UART peripheral in ring buffer mode  | 
| WDT Timeout | This is a WDT test application designed to demonstrate the communication timeout feature of the WDT application |