1.22 UART Echo Interrupt
This example application demonstrates how to use the UART peripheral to transfer a block of data in a non-blocking manner.
Description
This example shows the read and write operation over a UART in a non-blocking manner. The peripheral interrupt is used to manage the transfer. It receives 10 characters from the terminal window and echoes them back.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.
Path of the application within the repository is apps/uart/uart_echo_interrupt/.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| pic32ak_gc_curiosity.X | MPLABX project for Curiosity Platform Development Board and PIC32AK1216GC41064 General Purpose Dual In-Line Module (DIM) | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description | 
|---|---|
| pic32ak_gc_curiosity.X | Curiosity Platform Development Board and PIC32AK1216GC41064 General Purpose Dual In-Line Module (DIM) | 
Setting Up Curiosity Development Board
- Insert the GP DIM on to DIM slot of Curiosity Board
 - Connect the PKoB (J21) on the board to the computer using a USB type-C cable
 
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer
 - Connect to the “PICkit 4 On Board
                    Virtual COM Port” and configure the serial settings as follows:
- Baud : 115200
 - Data : 8 Bits
 - Parity : None
 - Stop : 1 Bit
 - Flow Control : None
 
 - Build and Program the application project using its IDE
 - See the following message in the
                        console:

 - Type 10 characters in terminal
 - Entered 10 characters is echoed back and LED is toggled