13.22.7.4 SET_CFG_2

There is a SET_CFG_2 message that is sent by the host dsPIC DSC to the MOSFET Gate Driver to configure the driver current limit blanking time. The SET_CFG_2 message may be sent to the devices at any time. The host is responsible for making sure the system is in a state that will not be compromised by sending the SET_CFG_2 message. The SET_CFG_2 message format is indicated in Table 13-6. The response is indicated in Table 13-7.