13.22.7.1 SET_CFG_0
There is a SET_CFG_0 message that is sent by the host dsPIC DSC to the MOSFET Gate Driver to configure the driver. The SET_CFG_0 message may be sent to the driver at any time. The host is responsible for making sure the system is in a state that will not be compromised by sending the SET_CFG_0 message. The SET_CFG_0 message format is indicated in Table 13-6 . The response is indicated in Table 13-7 .