The Bootloader project will have the
Fuse settings set to default except the BOOTPROT fuse
BOOTPROT is set to 4096 Bytes
(0xB) during production to protect the Bootloader from accidental
erase/writes.
The Fuse settings can be changed in
following ways:
The Bootloader provides a
separate command to program the Fuse Bits received from the host. Refer to
the Bootloader protocol documentation and respective host utility
documentation for more information.
The application can check the
Fuse bits during the boot-up and then program any change required using the
NVMCTRL peripheral
As fuse settings are placed in a
higher memory location in the Flash (User Row), the Fuse settings need to be
disabled for the application project, which will be boot-loaded since the size of
the binary file becomes too large when the fuse settings are enabled
When updating the Bootloader itself,
make sure that the fuse settings for the Bootloader application are also
disabled
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.