2.2.2 BER Receive Test Mode Setup
The BER Receive Test mode is set up using register A21 (GPO test register) with the
following settings:
| Bit# | Name | Description |
|---|---|---|
| 32 | GPO_select[5] |
(default: 0) |
| 31 | GPO_select[4] | |
| 30 | GPO_select[3] | |
| 29 | GPO_select[2] | |
| 28 | GPO_select[1] | |
| 27 | GPO_select[0] | |
| 23 | DIG_PN_Stream |
RX checks the accuracy of the sequence; if there is an error, the GPO pin is set; the PN generation starts with the TX/RX mode. Apply a power-down sequence to exit. |