2.4.2.1 PLL Reference Clock Source
The following sources are available from the reference clock menu.
- Dedicated Input Pad —The clock source is one of the four regular FPGA I/Os that have a dedicated path to the CCC. The Configure as differential option allows you to configure any dedicated Input Pad as differential I/O. The package pin names for the selected CCC location are displayed next to the dedicated pads.
- FPGA Fabric Input —The clock source can be one of the four input signals coming from the FPGA Fabric.
- Oscillators —The source is from the on-chip 50 MHz oscillator.