1.1.3.8 WDRV_WINC_AssocSSIDGet Function
WDRV_WINC_STATUS WDRV_WINC_AssocSSIDGet (
C
DRV_HANDLE handle, WDRV_WINC_SSID *const pSSID,
WDRV_WINC_ASSOC_CALLBACK const pfAssociationInfoCB
)
Summary
Retrieve the current association SSID.
Description
Attempts to retrieve the SSID of the current association.
Precondition
WDRV_WINC_Initialize should have been called. WDRV_WINC_Open should have been called to obtain a valid handle. A peer device needs to be connected and associated.
Parameters
Param | Description |
assocHandle | Association handle. |
pSSID | Pointer to buffer to receive the SSID if available. |
pfAssociationInfoCB | Pointer to callback function to be used when SSID is available. |
Returns
WDRV_WINC_STATUS_OK - pSSID will contain the SSID. WDRV_WINC_STATUS_NOT_OPEN - The driver instance is not open. WDRV_WINC_STATUS_INVALID_ARG - The parameters were incorrect.
WDRV_WINC_STATUS_REQUEST_ERROR - The request to the WINC was rejected or there is no current association. WDRV_WINC_STATUS_RETRY_REQUEST - The SSID is not available but it will be requested from the WINC.
Remarks
If the SSID is not currently known to the driver (stored within the WINC) a request will be sent to
the WINC and the return status will be WDRV_WINC_STATUS_RETRY_REQUEST. The callback function pfAssociationInfoCB can be provided which will be called when the WINC provides the association information to the driver. Alternatively the caller may poll this function until the return status is WDRV_WINC_STATUS_OK to obtain the SSID in pSSID.