8.13.6.2 PUF Operation Result Register

Name: PUF_ORR
Offset: 0x004
Reset: 0x00000000
Property: Read-only

Bit 3130292827262524 
 LOPNUM[7:0] 
Access RRRRRRRR 
Reset 00000000 
Bit 2322212019181716 
          
Access  
Reset  
Bit 15141312111098 
 RESEEDRRESEEDW       
Access RR 
Reset 00 
Bit 76543210 
 RCODE[7:0] 
Access RRRRRRRR 
Reset 00000000 

Bits 31:24 – LOPNUM[7:0] Last Operation Number

ValueNameDescription
0x00 IID_PUF_LO_PROGRESS An operation is in progress.
0x01 IID_PUF_LO_ENROLL The last operation was ENROLL.
0x02 IID_PUF_LO_START The last operation was START.
0x03 IID_PUF_LO_RECONSTRUCT The last operation was RECONSTRUCT.
0x4 Reserved Reserved
0x05 IID_PUF_LO_STOP The last operation was STOP.
0x06 IID_PUF_LO_GET_KEY The last operation was GET KEY.
0x07 IID_PUF_LO_UNWRAP The last operation was UNWRAP.
0x08 IID_PUF_LO_WRAP_GEN_RND The last operation was WRAP GENERATED RANDOM.
0x09 IID_PUF_LO_WRAP The last operation was WRAP.
0x0A–0x0E Reserved Reserved
0x0F IID_PUF_LO_GEN_RND The last operation was GENERATED RANDOM.
0x10 IID_PUF_LO_RESEED The last operation was RESEED.
0x11–0x1D Reserved Reserved
0x1E IID_PUF_LO_TEST_MEMORY The last operation was TESTMEMORY.
0x1F IID_PUF_LO_TEST_PUF The last operation was TESTPUF.
0x20 IID_PUF_LO_INITIALIZATION The last operation was INITIALIZATION.
0x21–0x2E Reserved Reserved
0x2F IID_PUF_LO_ZEROIZE The last operation was ZEROIZE.

Bit 15 – RESEEDR Reseed Required

ValueNameDescription
0 NO_ACTION No action required.
1 REQUIRED_ACTION The maximum number of DRBG2 requests has been done. A reseed must be performed before other operations can be done. This bit is the same as in PUF_SR.

Bit 14 – RESEEDW Reseed Warning

ValueNameDescription
0 NO_ACTION No action required.
1 RECOMMENDED_ACTION The DRBG reseed counter is close to its limit, it is recommended to reseed at the first suitable moment. This bit is the same as in PUF_SR.

Bits 7:0 – RCODE[7:0] Last Operation Result Code

ValueNameDescription
0x00 IID_PUF_OK The last operation was successful or an operation is in progress.
0xF0 IID_PUF_ERR_PRODUCT The provided activation code is not correct.
0xF1 IID_PUF_ERR_PRODUCT_PH2 The activation code in the second phase is not correct.
0xF2 IID_PUF_ERR_TRANSFER The provided activation code is corrupted.
0xF3 IID_PUF_ERR_TRANSFER_PH2 The activation code in the second phase is corrupted.
0xF4 IID_PUF_ERR_AUTH Authentication of the provided activation code failed.
0xF5 IID_PUF_ERR_AUTH_PH2 Authentication of the provided activation code failed in the second phase.
0xF6 IID_PUF_ERR_PUF_QUALITY Dedicated Embedded Static RAM PUF quality verification fails.
0xF7 IID_PUF_ERR_CONTEXT An incorrect or unsupported context is provided.
0xF8 IID_PUF_ERR_DESTINATION A data destination that was set is not allowed according to other settings and the current PUF state.
0xF9–0xFA Reserved Reserved
0xFB IID_PUF_FAILURE_DRBG2_ENTROPY DRBG2 Reseed or Instantiation failed (DRBG1 cannot provide entropy).
0xFC IID_PUF_FAILURE_DRBG1_ENTROPY The entropy test for DRBG1 failed.
0xFD IID_PUF_FAILURE_DRBG_HEALTH One or more of the DRBG health tests failed.
0xFE IID_PUF_FAILURE_SETTINGS Initialization cannot finish due to illegal values in PUF_HW_SETTINGS.
0xFF IID_PUF_FAILURE_SRAM PUF SRAM access has failed.