20.5.2.9 External Clock
The output clock (GCLK_GEN) of each Generator can be sent to I/O pins (GCLK_IO).
If GENCTRLn.OE is 0, the according I/O pin is set to an Output Off Value, which is selected by GENCTRLn.OOV. If GENCTRLn.OOV is '0', the output clock will be low. If this bit is '1', the output clock will be high.
In Standby mode, if the clock is output (GENCTRLn.OE = 1), the clock on the I/O pin is frozen to the OOV value if the Run In Standby bit of the Generic Control register (GENCTRLn.RUNSTDBY) is zero. If GENCTRLn.RUNSTDBY is '1', the GCLKGEN clock is kept running and output to the I/O pin.