6.1 Step 1: Review Configurations
This step displays a summary of the current Main and Peripherals settings that will be applied to all target devices.
- Device configurations are shown in collapsible detail lists and tables for easy review
- Chip access options can be configured
here:
- Password protection toggle—Opens the Enable Password Dialog
- Permanently lock the device toggle—Opens the Permanent Lock Dialog
- A Validation status card shows
whether the current configuration is valid:
Validated—The configuration is ready to apply
Fix configuration error(s)—One or more settings have errors that must be resolved before proceeding. Navigate to the Main Tab and/or Peripherals Tab to correct the invalid settings, then return to the Automation tab to continue.
- The Confirm button locks in the configuration for Step 1. It is disabled if there are validation errors or if automation is not in the Idle state.