1.4.3.35 MMHI_MIB_Get Function
C
MMHI_RESULT MMHI_MIB_Get(MMHI_MIB_INDEX mibIndex, MMHI_MIB_DATA* pData);
Summary
The MMHI_MIB_Get primitive gets the value of an attribute in the Host Interface Parameter Information Base (IB).
Description
MMHI_MIB_Get primitive is used to get the value of an IB.
Result is provided upon function call return, in the pData parameter.
Parameters
| Param | Description |
|---|---|
|
mibIndex |
Identifier of the Attribute to retrieve value. See MMHI_MIB_INDEX Enum |
|
pData |
Pointer to MMHI_MIB_DATA object where value will be returned. |
Returns
Result of get operation as a MMHI_RESULT Enum.
Example
MMHI_RESULT result;
MMHI_MIB_DATA value;
result = MMHI_MIB_Get(MIB_MIB_ID_MAC_CONFIG, &value);
if (result == MMHI_MIB_SUCCESS)
{
/* Read value */
}
Remarks
None.