1.2.12.4.14 SRV_QUEUE_ELEMENT Struct
C
typedef struct SRV_QUEUE_ELEMENT_tag
{
/* Pointer to the previous object of the queue */
struct SRV_QUEUE_ELEMENT_tag *prev;
/* Pointer to the next object of the queue */
struct SRV_QUEUE_ELEMENT_tag *next;
/* Element priority (only with priority queues) */
uint32_t priority;
} SRV_QUEUE_ELEMENT;
Summary
Queue element.
Description
This structure contains the data stored in each queue element.