1.2.2.4.7 SRV_PSNIFFER_SetPLCChannel Function

C

void SRV_PSNIFFER_SetPLCChannel
(
    uint8_t channel
);

Summary

Sets PLC channel to be used on PLC Sniffer.

Description

This function allows setting the right PLC channel to listed to. If misconfigured, no PLC frames will be seen.

Precondition

None.

Parameters

ParamDescription
channelThe PLC channel to listen to.

Returns

None.

Example

switch (command) {
    case SRV_PSNIFFER_CMD_SET_PLC_CHANNEL:
    {
        DRV_PLC_PHY_CHANNEL channel;
        
        channel = *(pData + 1);
        
        if ((appData.channel != channel) && (channel >= CHN1) && (channel <= CHN7_CHN8))
        {
            appData.channel = channel;
            
            /* Set channel configuration */
            appData.plcPIB.id = PLC_ID_CHANNEL_CFG;
            appData.plcPIB.length = 1;
            *appData.plcPIB.pData = channel;
            DRV_PLC_PHY_PIBSet(appData.drvPl360Handle, &appData.plcPIB);
            /* Update channel in PSniffer */
            SRV_PSNIFFER_SetPLCChannel(appData.channel);
        }
    }
    break;

    /* ... */
}

Remarks

This function is only available in PRIME PLC profile.