34.6.2.10 Channel Status

The Channel Status register (CHSTATUS) shows the status of the channels when using a resynchronized path. There are two Status bits in the CHSTATUS register for each of the available channels:

  • The CHSTATUSn.BUSYCH bit will be set when an event on the corresponding channel ‘n’ has not been handled by all event users connected to that channel.
  • The CHSTATUSn.RDYUSR bit will be set when all event users connected to the corresponding channel are ready to handle incoming events on that channel.