9.6.7.7 Loadaddr Built-in Function

The LOADADDR(section) built-in function returns the absolute LMA of the named section. This is normally returns the same address as ADDR, but it may be different if the AT attribute is used in the output section definition (see Sections Command).